Friday, December 20, 2013

Automotive sensors test



Today’s vehicles, whether a concept car or your commuter, are choke full of sensors and controls.  In the idealized world of the car designers these sensors and controls totally and completely monitor and control all the functions of the vehicle at all times.  Any problem will be reported in error codes.  Their subsequent remedies are detailed in service procedures.  Still for designer or servicer alike, sometimes these sensor inputs need to be verified.  One may want to have an actual temperature measurement, or a sensor voltage reading independent of the diagnostic system.
One of Agilent’s customers, Tracy, is a design engineer for automotive sensors and controls systems.  He helps us understand some of the challenges working with a vehicle platform.  In particular, there is a hard divide between the engine and the passenger compartment.  There are no port holes or service doors.  There is no easy way to run test leads, wires or thermocouples from the engine to the driver, so that he can see how the temperature or voltage behaves as the vehicle is driven through different conditions.


  


[Caption:  a thermocouple, blue wire, inside the engine compartment.  In an actual measurement, the wire will terminate inside the airbox, for  example, and not be visible to the camera.]



[Caption:  a connector where voltage measurement can be taken with test leads, or back probe pins.]



Using the Agilent WRC (wireless remote connectivity) meter, Tracy now can access the measurements inside the passenger compartment wirelessly.  It is simple and painless.  The thermocouple or test leads are connected to an Agilent handheld multimeter, which is secured inside the engine compartment with the hood closed.  The measurement results are transmitted via a Bluetooth adaptor to an Android tablet (or phone) inside the passenger compartment.  The Android app is free from Agilent or Google Play Store.  It takes only a few clicks to get going, much easier than any other alternatives.


20 comments:

  1. Thanks for the informative article. This is one of the best resources I have found in quite some time. Nicely written and great info, I really thank you for sharing it. Looking forward read more, great article. thanks for posting.
    MATLAB Assignment Help

    ReplyDelete
  2. Oh! This article has suggested to me many new ideas. I will embark on doing it. Hope you can continue to contribute your talents in this area. Thank you.
    run 3

    ReplyDelete
  3. Take a look at the list of the most essential things for living in a dormitory and pack your bags.

    ReplyDelete
  4. Our Online Essay Writer Service mission is to ensure clients are satisfied has ensured access to customer service 24/7 meant to address all issues relating to custom term papers and Online Nursing Essay Writing Services offered by the company.

    ReplyDelete
  5. Have always love this platform Beyonce lifestyle story

    Especially this one.
    Drake Lifestyle luxury


    Thanks for updates

    ReplyDelete
  6. QuickBooks Online is widely used by people who need to access their business from multiple locations and multiple devices. so if you still have the QBDT version then you can switch to QBO. It has all the features of QBDT along with its own features. you can shift your Company file with some easy steps. if you need assistance to switch to QBO then you can contact Quickbooks Enterprise Support.

    ReplyDelete

  7. township hack
    Township is an engaging internet game, Township cheats which offers a special blend of cultivating and town-building components

    ReplyDelete
  8. Your review is very great and useful for me…thank you
    sonic games

    ReplyDelete
  9. Their ensuing cures are definite in administration systems. Still for originator or servicer the same, in some cases these sensor inputs should be confirmed. One might need to have a genuine temperature Online Content Writing Services estimation, or a sensor voltage perusing free of the analytic framework.

    ReplyDelete
  10. This article is really fantastichttp Click game to play. thanks for sharing the valuable post.

    ReplyDelete
  11. Can Someone Do My Class Online For Me? Can I Pay Someone To Take My Class Online For Me? Try Us! Best Mentors Online is the best Online Class Help Company for you!

    ReplyDelete