Monday, February 10, 2014

Solar LED Street Light Test


Solar LED street lighting has been talked about more and more these days.  It adopts the green energy supply technology – photovoltaic (PV) panel with sun power that will never exhaust.
Another advantage of using LED lighting is that it consumes lower energy and has longer life compared to the old compact fluorescent lighting (CFL). Lower energy consumption also means there will be a decrease in carbon dioxide (CO2) emission, sulfur oxide or other waste that is harmful to the environment.  The average life span for the LED is approx. 50,000 hrs whereas the CLF is only 8,000 hrs. This indirectly helps to reduce the maintenance cost of replacing light bulbs.


Solar LED street lights got popular at remote locations where electricity is not available or irregular. Today, it is common in the urban areas with the independency of conventional power supply and the energy efficiency towards the green energy.

Figure 1  New Solar LED street light adjacent to the electricity street light


Solar LED street light consists of 5 main parts: Luminaire, solar panel, battery, pole and a system that consists of a module to integrate the LED driver function and the solar charger to battery. The electronic module is housed in the luminaire which is mounted at a few meters height. 
During the installation, a person has to climb on the pole and check on the electronic module for its complete functionality. This takes more than 10 minutes and has to be monitored by the person on the pole. By connecting to Agilent Wireless Remote Connectivity Solution, there can be one person monitoring measurement results on the ground while another person probes for readings using the Agilent handheld multimeter. 

Figure 2 Agilent wireless remote connectivity solution
 Sometimes, the worker needs to climb on the pole to check and monitor the PV panel, battery, or LED side parameter for any fault for extended hours. A wireless metering/monitoring device with data logging would help to save the time and effort of staying on the pole.

Using the Agilent Wireless Connectivity solution, the worker can now comfortably capture and monitor the measurement reading on the ground while the Agilent handheld multimeter can be easily secured on the pole with its hanging kit. The measurement results are transmitted via Bluetooth adaptor to an  Android tablet or phone of the worker for further analysis. 


22 comments:

  1. This information will explain you how to hack Instagram. Take a look.

    ReplyDelete
  2. All clients seeking assistance with our Term Paper Writing Help Services services are assured 24/7 access to the customer service department which addresses all the issues they may have on the Cheap Online Assignment Services being completed.

    ReplyDelete
  3. Have always love this platform Beyonce lifestyle story

    Especially this one.
    Drake Lifestyle luxury


    Thanks for updates

    ReplyDelete

  4. township hack
    Township is an engaging internet game, Township cheats which offers a special blend of cultivating and town-building components

    ReplyDelete
  5. Thank you for your detailed post. It's good to know about this LED street light test.
    surviv.io

    ReplyDelete
  6. Nice knowledge gaining article. This post is really the best on this valuable topic. best led track lighting

    ReplyDelete
  7. Thanks to the share from you that I have learned an interesting information apkxyz

    ReplyDelete
  8. Thank you for the informative content, It is really informative for my electric engineering assignment help Pakistan, in which I was unable to find relevant content & then I found this article of yours. It was really helpful for me, Thanks again.

    ReplyDelete
  9. With an mspy.com app installed on your kid's smartphone, you can easily see what they have in their website bookmarks. Definitely a useful app for parents, I must say

    ReplyDelete
  10. Don't need to worry about the
    getinkpreferred.com you will get an adequate knowledge for it.

    ReplyDelete
  11. It's very good post which I really enjoyed reading. It is not everyday that I have the possibility to see something like this.
    url of the apk

    ReplyDelete
  12. However, if the all in one solar LED street light is broken, how should it be repaired?

    hotstar app apkxyz

    ReplyDelete
  13. The article you have shared here very awesome. I really like and appreciated your work. I read deeply your article, the points you have mentioned in this article are useful
    url

    ReplyDelete
  14. Thanks for sharing this with us.i found it informative and interesting.

    How To Install And Play Call Of Duty

    ReplyDelete
  15. Thanks for sharing this with us.i found it informative and interesting.
    How To Hack Instagram account

    ReplyDelete
  16. Quickbooks is one of the best accounting software which have multiple accounting features. If you want to transfer quickbooks data to a new pc , you can create a backup file automatically or manually. This backup file will help you to retreive the lost data.

    ReplyDelete