Sunday, February 23, 2014

Maintenance and troubleshooting works in a ski resort

Every ski resort have their own electrical engineering team to monitor the operation of gondolas, ski lifts, kitchen, hotel, staff accommodations and all other buildings. This team of technicians and engineers are to be available everywhere and at all times to ensure that everything is working smoothly. During summer, maintenance and troubleshooting works are being done.

Dave Monminie is an electrical supervisor at Sunshine Village Ski and Snowboard Resort in Banff National Park. He came across Agilent’s website while searching for multimeter to replace his old Fluke 12 which he accidentally dropped from 30 feet up a ski lift tower. While researching, Dave also came across Ideal, Greenlee and Fluke’s meters, but thought that U1194A Handheld Clamp Meter was the one. But he then saw the U1213A Handheld Clamp Meter with Bluetooth connectivity and thought that it could be a very useful tool, and will be able to turn a 2-person job into a 1-person job.

Here are some examples given by Dave:

On our Great Divide lift here at Sunshine Village, there was a 10 amp breaker located inside our top operator's shack, wayyyyy up there out of sight, which was tripping. The circuit feeds 4 different branches which are outside, 10 meters or so to the ladder and up in the return station which looks much like the drive station below.
The Great Divide lift at Sunshine Village Ski and Snowboard Resort
Having just hiked for an hour and a half to the top, I was the only person available to troubleshoot. The problem was that when the breaker was reset, it would trip before I could get into position up in the station to take a measurement. Now, I could have disconnected all the branches, went down the ladder, flipped the breaker, climbed back up the ladder, placed the amp clamp on a wire, touched it to the power rail with my hand, and noted the amperage draw, but that creates arcing and sparking which our all too finicky electronics do not appreciate. If only I could see the display on a clamp meter measuring the amperage of one of the branch circuits all the way up in the station while I flipped the breaker down in the shack, I could find the problem all by myself. It'd be like I was in two places at once.

Mentoring is another area I’d find it useful. The doors to our lift control cabinets are pretty narrow, and definitely have room for only one pair of shoulders at a time. Having a second display, on my android phone, would allow me to see what my apprentice is seeing while measurements are being made.

Lift Control Cabinet at Sunshine Village Ski and Snowboard Resort
  
In regards to safety, our lift motor control cabinets are 480volts. It'd be much faster, safer and convenient to kill the incoming power, attach the meter leads inside the cabinet, close the doors and then power up to take measurements rather than have to change our clothes from snow gear to flash protection clothing and back again every time we need to open these doors.

Lift Motor Control Cabinet

Another thing we could have done more safely was when we recently suffered flood damage from an incredible amount of rain in the Bow Valley, Alberta. Our warehouse flooded and the distribution panel was approximately 3 feet under water. When the water eventually drained, we pressure washed the bus bars, set up fans and waited 3 days for everything to dry out, did continuity tests from phase to phase and phase to ground. Everything checked out... still, it would have been safer to energize the
distribution panel from the generator room outside and watch the readings from a safe distance.

 Flood at Bow Valley, Alberta

Dave is one of the winners of our Wireless Remote Connectivity application stories contest. He has some concern over meter’s operating temperature, as they will experience cold spell of -30 to -40 °C at least twice a year. Well Dave, check out our multimeter that is made for these extreme temperatures – U1273AX Handheld Digital Multimeter, 4.5 digit, OLED display. You don't have to hide them in your pockets anymore!



Congratulations Dave, and thanks for sharing your stories with us. 

22 comments:

  1. This post shares information on how to write a scientific paper taking into account its proper format.

    ReplyDelete
    Replies
    1. These cut-price Sennheiser over-ear headphones aren't just big on value, they're feature-rich too. The Bluetooth implementation is leading edge best budget bluetooth headphones. Best cheap wireless headphone deals: Skullcandy Ink'd Plus Wireless Earbuds. Wireless earcandy. Plantronics Backbeat Pro 2.

      Delete
    2. Wireless Keyboard & Mouse Combo KEY FEATURES FAMILIAR KEYBOARD LAYOUT No learning curve involved wireless keyboard and mouse. Wifi keyboard price and mouse price in Pakistan are low, including wireless

      Delete
  2. The information you shared is very helpful, thank you for sharing.
    read manga online

    ReplyDelete
  3. We are the best writing company providing College Term Paper Writing Services papers over 15 years, we have been operational as we have assisted thousands of students with their Online Custom Research Paper Services.

    ReplyDelete
  4. Have always love this platform Beyonce lifestyle story

    Especially this one.
    Drake Lifestyle luxury


    Thanks for updates

    ReplyDelete
  5. Learn about Best Essay Writing Services that are congenial to your needs.Writers delve deeper into concepts about Custom Dissertation Writing, and the qualities to consider when writing Best Dissertation Writing Service.

    ReplyDelete
  6. cheats for pixel car racer
    Pixel Car Racer is another racing game for the iOS and Android stages. It has a portion of the more point by point tuning you’ll find in any game, regardless of the straightforward pixel designs.

    ReplyDelete
  7. Artillery is also used to blast remote avalanche paths that affect ski runs .

    website

    ReplyDelete
  8. brawl stars hack apk
    SUPERCELL'S 2020 BRAWL STARS CHAMPIONSHIP FEATURES OPEN COMPETITION, MONTHLY FINALS, GLOBAL FORMAT AND OVER $1 MILLION IN PRIZES

    ReplyDelete
  9. The article you have shared here very awesome. I really like and appreciated your work. I read deeply your article, the points you have mentioned in this article are useful
    here

    ReplyDelete
  10. hhow do you get free robux
    Roblox is a MMO (greatly multiplayer on the web) social gaming stage. In excess of 62 million players utilize the Roblox game every mont

    ReplyDelete
  11. he effort you made to share the knowledge. The topic here i found was really effective to the topic which i was researching for a long time.

    How To Downgrade iOS 13.1.1 or iPadOS 13.1.1

    ReplyDelete
  12. When the sunset did not settle down. When dawn is still not quiet. Let me have a chance, I will see this belief is completely a ray of sunshine, Shining into that darkness leads the way to want to pull me back to your side.geometry dash

    ReplyDelete
  13. Wireless connectivity has really made our lives easy so thumbs up from me to you for posting this here. However, if you like reading about the new mortgage rates austin then do give a read to this one.

    ReplyDelete
  14. Save your personal information in Wallets. Editing, shred files and clean your Windows History. Your directories are protected using the 256bit Blowfish Encryption method.
    windows 7 prodotto chiave di attivazione Archivi
    https://nonsugar.info/hack-latest-tool/19112-filezilla-log-out-of-facebook.html

    ReplyDelete
  15. 123 hp com envy5640 Wireless Setup for 123 HP Envy 5640 Wi-Fi Printer & WPS Network for user credentials to Set-up 123HP Envy 5640 Wireless Set up.

    ReplyDelete