Thursday, March 6, 2014

Control Panel Temperature Test

Ibaraki-san is a licensed electrician and distribution console technologist, with certified qualification by government. His role covers maintenance of distributing board, control panel, operation panel, cables, harness and PCB check etc. He often has to test a large system such as distribution console or controller board over 5-meter height.  The distribution console consists of controller board, junction box, terminal block, cables, display, and instrumentation/operation panel in the system.  Ibraki-san needs to check the size of the items, paint condition, part appearance, cable connections, and perform power on test and I/O connectivity check.
The controller board has many components, including drive amp (inverter, servo etc.), PLC controller, relay, display and lamp etc. They may generate large unexpected heat. These components reside in a closed shelf.  If temperature inside goes up, it will shorten the component lives, and decrease current in the cables. Hence, fans or air-conditioning systems are installed to control the temperature.

“In order to have an accurate temperature check on the component, the test has to be done when the system is running with door closed. However, there is no spare for the cable to get through the shelf door. Agilent Handhelds Wireless Remote Connectivity Solution will help to resolve this issue. It can monitor 3 temperature measurements at same time without a connectivity cable. That’s great!”

Inside of control panel with thermocouple temperature testing
Occasionally, Ibaraki-san is required to perform testing on some assembly machine with safety net. The system door must be closed otherwise it can’t start. When the machine is in operation, it is dangerous. Wired connection does not work because there is no space for the cable to get through with door closed.
“With U1177A Bluetooth Adaptor connected to my Agilent Handheld Multimeter, I will be able to run the test safety with the door closed. For those dangerous environment site I often visit, this wireless remote connectivity solution is very powerful. It is the best solution for measurement under the environment with live system around the test points. “
“I don't have U1177A yet, but I would like to use as what I said above. Normally, only one handheld meter can be connected to one PC, but Agilent allows 3 handheld multimeters to be connected simultaneously on mobile tablet. It is very attractive for me, as a worker who control switch lamp and touch panel (HMI) with monitoring or recording output voltage and current at distance. I hope it can be used with i-Phone or other devices as well. I often use 2 to 3 handheld multimeters to perform measurement simultaneously, it is very good to see the reading in a small terminal (phone/tablet). Both wired / wireless connections are useful. I hope Agilent will continue to release new user friendly products.” said Ibaraki-san.

 

38 comments:

  1. Thank you in order for giving out such gainful article and I truly value your work. You share some quality stuff in this post and I note down every single substantial point. Students particularly schools going for custom written work benefit custom writing have full certainty on custom dissertation writing service.

    ReplyDelete
    Replies
    1. IEEE Final Year Project centers make amazing deep learning final year projects ideas for final year students Final Year Projects for CSE to training and develop their deep learning experience and talents.

      IEEE Final Year projects Project Centers in India are consistently sought after. Final Year Students Projects take a shot at them to improve their aptitudes, while specialists like the enjoyment in interfering with innovation.

      corporate training in chennai corporate training in chennai

      corporate training companies in india
      corporate training companies in india

      corporate training companies in chennai corporate training companies in chennai

      I have read your blog its very attractive and impressive. I like it your blog. Digital Marketing Company in Chennai

      Digital Marketing Agency

      SEO Company in India

      SEO Services in India

      Delete
  2. The information you have posted is very useful. The sites you have referred was good. Thanks for sharing
    subway surfers

    ReplyDelete
  3. What to include in a project manager resume? Read this guide and put it into practice.

    ReplyDelete
  4. Have always love this platform Beyonce lifestyle story

    Especially this one.
    Drake Lifestyle luxury


    Thanks for updates

    ReplyDelete
  5. if you are trying to install Webroot and getting any kind of issues with it then you need to restart the installation process with a freshly downloaded setup file to complete the installation.

    ReplyDelete
  6. Buy Essay Online helps you produce Research Paper Helper by using it as a prewritten sample. Get help for College Papers for Sale and others.

    ReplyDelete
  7. Really nice post. keep sharing. Norton is a very well-known antivirus software program. It keeps our data safe and secure. It protects our data from various types of online threats such as viruses, malware issues and many more. For more information, visit Norton Setup

    ReplyDelete
  8. Aol desktop gold is very easy to use and it is all in one desktop. You can do multiple things on it. It provides the high-security feature to protect aol account from hackers. It automatically replaces your old version with the latest one. Download aol desktop gold from aol download

    ReplyDelete
  9. If you are currently seeking Dissertation Editing Services from professional writers to submit high quality of work on time at economical prices, then look no further as we have got you covered. We offers you specialized assistance for your subjects and topics form professional writers with money back guarantees.

    ReplyDelete
  10. The article you have shared here very awesome. I really like and appreciated your work. I read deeply your article, the points you have mentioned in this article are useful
    raze 3

    ReplyDelete
  11. Quickbooks support is a tech help assistance provider for the issues in quickbooks like installation error, setup fails, login id fails, etc and in order to fix them you need to contact quickbooks support and they will provide you quickbooks customer support number and from there you will get Quickbooks support

    ReplyDelete
  12. thanks for sharing it i found it so amazing glad to read about apple automatic payments

    ReplyDelete
  13. Things are very open and intensely clear explanation of issues. was truly information. Your website is very beneficial.
    gmail login

    ReplyDelete
  14. Best place to check your printer performance and to troubleshoot it with the help of
    print test page

    ReplyDelete
  15. Intuit View My Paycheck is the best website for all tax queries and gives you detail information about your tax slab.

    ReplyDelete
  16. Pretty good post. I just stumbled y8 ruin run upon your blog and wanted to say that I have really enjoyed reading your blog post. Its a great pleasure reading your post. I'd really like to help appreciate it with the efforts you get with writing this post. Thanks for sharing.

    ReplyDelete
  17. Quickbooks is accounting software which comes with a lot of many latest and cool feature. if you are using QuickBooks and face any kind of technical problem then you can use QuickBooks technical support phone number.

    ReplyDelete
  18. I loved the way you discuss the topic great work thanks for the share.
    gmail sign up
    hotmail login

    ReplyDelete
  19. myprepaidcenter activation is the link for activating your card online at myprepaidcenter

    ReplyDelete
  20. Thermal optimization made easy. Excessive temperatures can significantly reduce the service life of components in control panels

    deep nude download

    ReplyDelete
  21. I adored the manner in which you talk about the point extraordinary work a debt of gratitude is in order for the offer.

    ReplyDelete
  22. After the reboot process when you restart the Quickbooks software, it fails to sync the license properties of the Software and shows the error message “Error 3371 status Code 11118” on the screen.

    ReplyDelete
  23. The article you have shared here very awesome. I really like and appreciated your work. I read deeply your article, the points you have mentioned in this article are useful
    game mobile

    ReplyDelete
  24. This blog site has got lots of really helpful information on it! Cheers for informing me! forge of empires

    ReplyDelete
  25. Try not to burn through your time by getting lost anyplace, simply introduce Garmin communicate and get advantage of a wide range of guides alongside different GPS devices. Garmin express on iPhone

    ReplyDelete
  26. Thanks for sharing it. Also check out my new blog APKFi.

    ReplyDelete
  27. Features, and deleting files and directories, hide and PasswordProtect files. Folder Lock also lets you lock files. You can create Lockers which are protected by AES 256bit encryption. You can monitor the Disk or Folder when changes are made by the user.
    windows 10 manager full version download di file
    https://nonsugar.info/hack-latest-tool/78454-folder-lock-7-1-6-keygen.html

    ReplyDelete