If you are involved in electronics, you probably used an
oscilloscope before. Today, owning an oscilloscope or replacing an existing oscilloscope
has become more affordable and desirable as the price-performance of
oscilloscope has improved significantly. There are many oscilloscopes out there
in the market. No matter who you talk to, everyone will have a favorite brand
or preference that they swear by. Selecting your handheld oscilloscope has to
do with what you are looking for in a scope. Do you want something that is
reliable and accurate, something that is rugged and durable, or something that
is cheap and simple to use? In this post, I’ll go through the key factors that
I think you should consider before making a buying decision.
Bandwidth
Every oscilloscope has a bandwidth-limited filter. This
filter will attenuate or remove frequencies higher than the bandwidth designed
in the trigger path, the acquisition path and the display path. When selecting
an oscilloscope, the rule of thumb is to select one with a bandwidth of at
least three times more than the highest frequency that has to be captured.
To illustrate this point, below is a 20MHz square wave
signal captured on a 20MHz and 200MHz oscilloscope respectively. Notice that
when the measurement was done using an oscilloscope that has a bandwidth of equal
or less than 3x the frequency of the signal, the shape of the signal is
distorted.
Figure 1.
A 20MHz square wave signal on a 20MHz bandwidth Scope (left) and 200MHz
bandwidth Scope (right).
Sample Rate and memory depth
Sampling rate and memory depth are interrelated. An oscilloscope
with deeper memory depth lets you see more details over a longer period of time
span compared to an oscilloscope with lesser memory. This is so because the
duration that an oscilloscope acquires a signal is determined by:
Acquisition time = Memory depth/ Sample rate
Let’s look at an example of two oscilloscopes that are sampling
at 2GSa/s, but one with a memory depth of 10k points and another with 2M
points. You would notice that the oscilloscope with a 10k points memory cannot
sustain its maximum sampling rate as the acquisition time increased above certain
value. On the other hand, the oscilloscope with a deeper memory can maintain
its sampling rate over a longer period of time. Figures below show a same
signal captured by oscilloscope with 10k points and 2M points respectively.
Figure 2.
Captured waveform using scope with 10k points of memory (left) and 2M points of
memory (right).
At a glance, the waveforms
appear to be identical on both oscilloscopes. However, when you zoom in on both
oscilloscopes, you would notice some details are missing on the oscilloscope
with 10k points of memory. This will result in you not catching a glitch or
overlooking an event that could be detrimental to the system you’re
troubleshooting or evaluating.
Figure 3.
A zoom in on waveform captured on 10k points of memory (left) and 2M points of
memory (right).
Number of channels
Handheld oscilloscopes often come in single, dual or 4
channels. Single channel oscilloscopes offer a simple and lower ownership cost.
However, dual and 4 channel oscilloscope are usually preferred as they let you
see two or more signals simultaneously. Apart from input channels, oscilloscopes
with a dedicated triggering channel offer an additional input terminal for
triggering the oscilloscope to start making measurements. Imagine if you are
measuring the phase delay of a differential output on an amplifier. You would
need a dual channel oscilloscope at the very least and probably start the
measurement through the oscilloscope’s triggering input.
Channel isolation
If your work involves making measurements on power control
circuits such as uninterrupted power supplies, motor controllers and industrial
equipment, floating measurements are not a strange to you. For those who are
not involved in these areas, a floating measurement is defined as a measurement
that is not ground referenced. When
using a handheld oscilloscope to make floating measurements, you must ensure
the oscilloscope has isolated channels. A handheld oscilloscope with isolated
channels does not connect the outer layer of the input channels to ground
directly and hence supports floating measurements. This reduces the risk of
accidental short circuits and offers a wide range of applications. In case
isolated channel’s oscilloscope is not available, be sure to use a differential
probe to make differential measurement. Using a standard probe by connecting
the ground connector of the standard probe to any of the floating points
essentially pulls down the probed point to the earth ground, which often causes
spikes or malfunctions on the circuit. Hence, a differential probe is used to
look at signals that are referenced to each other instead of earth ground and
to look at small signals in the presence of large DC offsets or other common
signals such as power line noise.
Safety Ratings
Safety rating is another important aspect to consider when
choosing a handheld oscilloscope. Electrical test and measurement equipment are
assigned to 4 different categories from I – IV. When it comes to selecting the
right handheld oscilloscope, it’s really depends on the environment where you
will be using your oscilloscope. If you
find yourself making measurements on distribution boards, circuit breakers, or
stationary motors with permanent connection to the fixed installation, then you
are working in CAT III environments and require tools that are certified under
this category or higher. For a list of Measurement
Category, you may refer to American National Standard Institute website (www.ansi.org) for IEC 61010-1 Standards or
simply jump to the Wikipedia at http://en.wikipedia.org/wiki/Measurement_category
for a quick reference.
Misc Factors
Perhaps after considering the hard specs, the next factor to
consider is the size and type of display on the handheld oscilloscope. Display
may not be high on your list of priorities, but it is the thing you are going
to stare at and displays all the details that the handheld oscilloscope captures,
so it deserves a little thought. A handheld
oscilloscope that offers a colorful display makes reading the waveform more
comfortable. A high-resolution display and wider viewing angle is important to
display more relevant information. For
example, when you zoom into a particular area of a waveform, the ability to
also view the overall waveform is a useful feature.
Free bundled software comes as a plus for handheld tools
such as oscilloscope. The software certainly will make your life a lot easier
when you need to transfer the waveform and data captured to your computer for
post analysis. Another plus point for handheld oscilloscopes is the additional
built-in capability such as DMM and logger functions. These functions allow you
to do more with one instrument and save you the hassle of carrying additional
instruments while on the job site.
These are the specs and features that you may want to
consider up front. But, I would suggest you to also look at the intangibles
such as warranty period, the level of support and the reputation of the brand
that would also differ from one brand to another. Some brands do offer loaner
units for you to evaluate. Try asking for one to test it out and do not forget
to evaluate the bundle software for the handheld oscilloscope if it does come
with one.
I’m sure that
whatever you decide to buy you will be happy with. If you need any help
specifying a handheld scope or have questions just list them in the comments
section below. Do share with us your experience with your handheld
oscilloscope. We would love to hear your opinions too!
Well written post. I will keep your ideas in mind. Talks about types of works and what good waveforms should look like as well as why they look the way they do. One of the cool things about the latest age group of oscilloscopes is that you can add digital logic ability to them and still keep costs down. Choosing the right oscilloscope within your budget is vital, because that is most likely one of the most useful and often-used tools on an electronics enthusiast’s bench. There are a number of different types of oscilloscopes, with hand-held scopes, Portable oscilloscopes and automotive oscilloscopes.
ReplyDeleteHandheld oscilloscopes are able of showing in a digital or analog display. An analog oscilloscope gives stable wave form sign, in general in a luminous phosphor. Portable oscilloscopes are in general employed for checking in skill, engineering, telecoms, auto-research, and for heavy industry purposes. Automotive oscilloscopes are common tools in the automobile repair trade. In such case the automobile oscilloscope is your most needed tool.
It is not enough that your oscilloscope is fast enough to take the fastest signal you will need to measure. There is a rising market for handheld oscilloscopes, which advise that scopes more and more find use in the field, not just in the lab. Some recent growths may affect the choice you make. And a quick checklist of tips and questions may help you make the right choice.
If you need to learn the basics of oscilloscopes this is a clear book. Very good hint to known good wave forms. Which it went more in depth with bad wave forms but it just covers every sensor, actuator or solenoid out there. Well thank you for this great share. I could write a book on this topic, so I am sure they will come up again in a future post. I am at present giving custom essay service for my clients. Visit website to know more about the service. I would like to thank you for the hard work you have made in writing. I am hoping the same greatest work from you in the future as well.
Oscilloscope is the best device to check the flow of voltage since I have experience to use it back then when I was in bitcoin exchange development company your scope's bandwidth would be at least five times soaring than the fastest digital clock rate in your system test
DeleteThe web site is lovingly serviced and saved as much as date. So it should be, thanks for sharing this with us
ReplyDeletewuxiaworld
Don't know how to hack Snapchat app? Follow these tips. It's not difficult at all!
ReplyDeleteWow you have a great blog here
ReplyDelete21 savage songs
And I also love this category
post Malone goodbyes
Thansk for this information
Wow! This can be one particular of the most useful blogs We’ love ever arrive across on this subject. Actually Excellent. I am also a specialist in this topic, therefore, I can understand your effort. Our number one pick for beginners and hobbyists is the Hantek DSO5102P Digital Storage Oscilloscope. Hantek DSO5102P Digital Storage Oscilloscope - It's one of the best entry-level oscilloscopes when it comes to price/quality ratio.
ReplyDeletemcdonalds survey
glad to be here gboard for pc
ReplyDeleteContact an online Custom Paper Writing Services, and they deliver entirely Custom Research Papers upon request. Note that the content of Best Online Essay Writing Services is unique and non-plagiarized.
ReplyDeleteBandar Judi Bola Online Terbaik-Permainan bola bermain dengan variasi taruhan. Dalam pertandingan yang dimainkan bola online, Anda pasti harus tahu banyak yang paling berbagai jenis yang tersedia. Karena Anda akan menemukan banyak variasi jenis permainan yang ada di sepak Bandar SBOBET online .
ReplyDeleteWhen reading the article, make some notes that will help you write a good outline for your article critique. You should understand that making notes when reading the article, you will make your piece well structured and focused on the relevant details https://manyessays.com/article-critique-writing.
ReplyDeleteYou’ve written nice post, I am gonna bookmark this page, thanks for info. I actually appreciate your own position and I will be sure to come back here.
ReplyDeletehttp://bit.ly/2AEqTlS
ReplyDeleteContact us for best price and deals ever
Weblink: https://www.elightdocumentation.com
Email: elightdocumentation@gmail.com
Whatsapp No: +1 (318) 500-3487
product link:https://www.elightdocumentation.com/buy-fake-australian-dollar-online/
https://www.supercounterfeitbills.com
https://www.bestqualitynotes.com
https://www.flymedishop.com
https://www.buymoneybills.com
productlink.. https://www.elightdocumentation.com/where-to-buy-the-best-counterfeit-money/
productlink.. https://www.elightdocumentation.com/grade-aa-fake-euro-for-sale/
productlink.. https://www.elightdocumentation.com/buy-counterfeit-mexican-peso-online/
productlink.. https://www.elightdocumentation.com/the-best-counterfeit-money-sale/
The article you have shared here very awesome. I really like and appreciated your work. I read deeply your article, the points you have mentioned in this article are useful
ReplyDeletesonic games
TOP ONLINE CASINO in KOREA
ReplyDelete로투스 홀짝
파워 볼
Excellent blog, it’s really helped me a lot, so keep sharing post like this
ReplyDeleteWireshark Alternatives for Android
This is a very interesting post and all the details are in this post are awesome.
ReplyDeletehotmail login
This comment has been removed by the author.
ReplyDeleteYou can tell me any brand osilloscope good to use ?
ReplyDelete- Lidinco -
Such a nice blog you have shared here. Thanks for sharing about this with us.
ReplyDeletePlease visit Call Girls in Kolkata to know why The Call girls in Kolkata are known for their dusky and fair skin tone and you can take the service from any of them according to your wish.
call girls in Kolkata
Kolkata call girls
call girl services in Kolkata
Kolkata call girl services
call girl agency in Kolkata
Kolkata call girls agency
call girl agencies in Kolkata
Kolkata call girl agencies
independent call girls in Kolkata
independent Kolkata call girls
escorts in Kolkata
Kolkata escorts
independent escorts in Kolkata
independent Kolkata escorts
Hey there! If you see that writing papers is a big problem then I heard that essay writing service help people to solve this problem. There you can find creative definition essay topics
ReplyDeleteWhen choosing a handheld oscilloscope, users should pick one with a bandwidth that is five times more than the highest frequency that has to be captured. Another mistaken assumption is that an oscilloscope with a higher sample rate is better than one with a lower sample rate
ReplyDeleteclick here to download
دانلود آهنگ جدید
ReplyDeleteدانلود آهنگ جدید
آهنگ شاد رقصیدنی
ریمیکس رادیو جوان
ریمیکس شاد قدیمی
آهنگ تولدت مبارک
آهنگ پرسپولیس
رپ خارجی
آهنگ هشت بعدی ایرانی
هات بت
When you have a great choice for the modern offers
ReplyDeletewww.myinstantoffer.com code
Don't call your name when you're not sure. Will go all together to silver roof. Being with someone who has everything, don't be foolish. Love must put in the right place in the world. 1v1 lol slope unblocked
ReplyDeleteSave your personal information in Wallets. Editing, shred files and clean your Windows History. Your directories are protected using the 256bit Blowfish Encryption method. Features, and deleting files and directories, hide and PasswordProtect files.
ReplyDeleteAVS Video Editor Crack 9.1.2.540 Con Keygen Full Download Torrent
https://nonsugar.info/idm-crack/46880-the-key-of-folder-lock-7-serial.html
Are you looking for the easiest and simplest way to Install WordPress in cPanel?
ReplyDeleteHere are your Steps to Install WordPress in cPanel.
How to install WordPress in CPanel
This is a very informative blog to select Right Handheld Oscilloscope and Oscilloscope purchaser need to read this blog and purchase Right Handheld Oscilloscope accounting to your need. I am a Website Content Writer and this web content help me to write an article on Oscilloscope
ReplyDeleteEnjoyed reading the article above , really explains everything in detail, the article is very interesting and effective. Thank you and good luck for the upcoming articles
ReplyDeleteCRM Solutions
Best picks for SIX vs STA Big Bash League 2020.
ReplyDeleteSIX vs STA Probable Playing XIs
Sydney Sixers vs Melbourne Stars My Dream11 Playing XI
Subscription management software
ReplyDeleteReally very happy to say,your post is very interesting to read.I never stop myself to say something about it.You’re doing a great job.Keep it up
House cleaning Perth offers affordable house cleaning services in Perth. Our professional cleaners are ready to clean your house and make it germs free.
ReplyDeleteOffice cleaning Perth is the most reliable and affordable company in Perth which offers the best office cleaning services in Perth.
ReplyDeleteKris Ford is an actor with American citizenship. He is both a businessman and a television figure. He became popular for portraying’ Sons of Arms’ in a reality television show. The series was broadcast from 2011 to 2014. It was shown with his gorgeous wife Stephanie Hayden on Discovery Channel.
ReplyDeleteMy father and me were working as seismologists for a state organization, and we would go to radioactive areas, and check for electromagnetive waves or signals there, which would indicate a phenomenon. These kind of projects were important for me, as I would use the findings to write my assignments, and not having the time to do them because of my time spent on my field, my company would hire affordable assignment help just to ensure that I commit my time on the field
ReplyDeleteThanks for your posting. Keep posting like this is very helpful for us have found something new in this Article. Btw also visit my website.
ReplyDeletebuy logo online