Sunday, May 18, 2014

How to Select the Right Handheld Oscilloscope?

If you are involved in electronics, you probably used an oscilloscope before. Today, owning an oscilloscope or replacing an existing oscilloscope has become more affordable and desirable as the price-performance of oscilloscope has improved significantly. There are many oscilloscopes out there in the market. No matter who you talk to, everyone will have a favorite brand or preference that they swear by. Selecting your handheld oscilloscope has to do with what you are looking for in a scope. Do you want something that is reliable and accurate, something that is rugged and durable, or something that is cheap and simple to use? In this post, I’ll go through the key factors that I think you should consider before making a buying decision.

Bandwidth
Every oscilloscope has a bandwidth-limited filter. This filter will attenuate or remove frequencies higher than the bandwidth designed in the trigger path, the acquisition path and the display path. When selecting an oscilloscope, the rule of thumb is to select one with a bandwidth of at least three times more than the highest frequency that has to be captured.

Oscilloscope bandwidth = Highest frequency component to be measured * 3

To illustrate this point, below is a 20MHz square wave signal captured on a 20MHz and 200MHz oscilloscope respectively. Notice that when the measurement was done using an oscilloscope that has a bandwidth of equal or less than 3x the frequency of the signal, the shape of the signal is distorted.

Figure 1. A 20MHz square wave signal on a 20MHz bandwidth Scope (left) and 200MHz bandwidth Scope (right).


Sample Rate and memory depth
Sampling rate and memory depth are interrelated. An oscilloscope with deeper memory depth lets you see more details over a longer period of time span compared to an oscilloscope with lesser memory. This is so because the duration that an oscilloscope acquires a signal is determined by:

Acquisition time = Memory depth/ Sample rate

Let’s look at an example of two oscilloscopes that are sampling at 2GSa/s, but one with a memory depth of 10k points and another with 2M points. You would notice that the oscilloscope with a 10k points memory cannot sustain its maximum sampling rate as the acquisition time increased above certain value. On the other hand, the oscilloscope with a deeper memory can maintain its sampling rate over a longer period of time. Figures below show a same signal captured by oscilloscope with 10k points and 2M points respectively.

Figure 2. Captured waveform using scope with 10k points of memory (left) and 2M points of memory (right).

At a glance, the waveforms appear to be identical on both oscilloscopes. However, when you zoom in on both oscilloscopes, you would notice some details are missing on the oscilloscope with 10k points of memory. This will result in you not catching a glitch or overlooking an event that could be detrimental to the system you’re troubleshooting or evaluating.

Figure 3. A zoom in on waveform captured on 10k points of memory (left) and 2M points of memory (right).


Number of channels
Handheld oscilloscopes often come in single, dual or 4 channels. Single channel oscilloscopes offer a simple and lower ownership cost. However, dual and 4 channel oscilloscope are usually preferred as they let you see two or more signals simultaneously. Apart from input channels, oscilloscopes with a dedicated triggering channel offer an additional input terminal for triggering the oscilloscope to start making measurements. Imagine if you are measuring the phase delay of a differential output on an amplifier. You would need a dual channel oscilloscope at the very least and probably start the measurement through the oscilloscope’s triggering input.

Channel isolation
If your work involves making measurements on power control circuits such as uninterrupted power supplies, motor controllers and industrial equipment, floating measurements are not a strange to you. For those who are not involved in these areas, a floating measurement is defined as a measurement that is not ground referenced.  When using a handheld oscilloscope to make floating measurements, you must ensure the oscilloscope has isolated channels. A handheld oscilloscope with isolated channels does not connect the outer layer of the input channels to ground directly and hence supports floating measurements. This reduces the risk of accidental short circuits and offers a wide range of applications. In case isolated channel’s oscilloscope is not available, be sure to use a differential probe to make differential measurement. Using a standard probe by connecting the ground connector of the standard probe to any of the floating points essentially pulls down the probed point to the earth ground, which often causes spikes or malfunctions on the circuit. Hence, a differential probe is used to look at signals that are referenced to each other instead of earth ground and to look at small signals in the presence of large DC offsets or other common signals such as power line noise.

Safety Ratings
Safety rating is another important aspect to consider when choosing a handheld oscilloscope. Electrical test and measurement equipment are assigned to 4 different categories from I – IV. When it comes to selecting the right handheld oscilloscope, it’s really depends on the environment where you will be using your oscilloscope.  If you find yourself making measurements on distribution boards, circuit breakers, or stationary motors with permanent connection to the fixed installation, then you are working in CAT III environments and require tools that are certified under this category or higher. For a list of Measurement Category, you may refer to American National Standard Institute website (www.ansi.org) for IEC 61010-1 Standards or simply jump to the Wikipedia at http://en.wikipedia.org/wiki/Measurement_category for a quick reference.

Misc Factors
Perhaps after considering the hard specs, the next factor to consider is the size and type of display on the handheld oscilloscope. Display may not be high on your list of priorities, but it is the thing you are going to stare at and displays all the details that the handheld oscilloscope captures, so it deserves a little thought.  A handheld oscilloscope that offers a colorful display makes reading the waveform more comfortable. A high-resolution display and wider viewing angle is important to display more relevant information.  For example, when you zoom into a particular area of a waveform, the ability to also view the overall waveform is a useful feature.
Free bundled software comes as a plus for handheld tools such as oscilloscope. The software certainly will make your life a lot easier when you need to transfer the waveform and data captured to your computer for post analysis. Another plus point for handheld oscilloscopes is the additional built-in capability such as DMM and logger functions. These functions allow you to do more with one instrument and save you the hassle of carrying additional instruments while on the job site.
These are the specs and features that you may want to consider up front. But, I would suggest you to also look at the intangibles such as warranty period, the level of support and the reputation of the brand that would also differ from one brand to another. Some brands do offer loaner units for you to evaluate. Try asking for one to test it out and do not forget to evaluate the bundle software for the handheld oscilloscope if it does come with one.


I’m sure that whatever you decide to buy you will be happy with. If you need any help specifying a handheld scope or have questions just list them in the comments section below. Do share with us your experience with your handheld oscilloscope. We would love to hear your opinions too!

92 comments:

  1. Well written post. I will keep your ideas in mind. Talks about types of works and what good waveforms should look like as well as why they look the way they do. One of the cool things about the latest age group of oscilloscopes is that you can add digital logic ability to them and still keep costs down. Choosing the right oscilloscope within your budget is vital, because that is most likely one of the most useful and often-used tools on an electronics enthusiast’s bench. There are a number of different types of oscilloscopes, with hand-held scopes, Portable oscilloscopes and automotive oscilloscopes.
    Handheld oscilloscopes are able of showing in a digital or analog display. An analog oscilloscope gives stable wave form sign, in general in a luminous phosphor. Portable oscilloscopes are in general employed for checking in skill, engineering, telecoms, auto-research, and for heavy industry purposes. Automotive oscilloscopes are common tools in the automobile repair trade. In such case the automobile oscilloscope is your most needed tool.
    It is not enough that your oscilloscope is fast enough to take the fastest signal you will need to measure. There is a rising market for handheld oscilloscopes, which advise that scopes more and more find use in the field, not just in the lab. Some recent growths may affect the choice you make. And a quick checklist of tips and questions may help you make the right choice.
    If you need to learn the basics of oscilloscopes this is a clear book. Very good hint to known good wave forms. Which it went more in depth with bad wave forms but it just covers every sensor, actuator or solenoid out there. Well thank you for this great share. I could write a book on this topic, so I am sure they will come up again in a future post. I am at present giving custom essay service for my clients. Visit website to know more about the service. I would like to thank you for the hard work you have made in writing. I am hoping the same greatest work from you in the future as well.

    ReplyDelete
    Replies
    1. Oscilloscope is the best device to check the flow of voltage since I have experience to use it back then when I was in bitcoin exchange development company your scope's bandwidth would be at least five times soaring than the fastest digital clock rate in your system test

      Delete
    2. Hi there, A bunch of thanks for sharing such valuable information & experience with us. We are livecoupons.net! Best place for coupons.

      Delete
    3. Lots of good answers to this question! I am posting a response taken from my blog: 

      Innovation…The word conjures up images in one’s mind. Perhaps you think about companies like Apple Computer, or great individuals like Thomas Edison, or out-of-the-box thinkers like Albert Einstein. I bet if you created a list, the list would be filled with many individuals, but only a handful of companies. Why is that? 

      I think part of the reason can be illustrated by way of example. Microsoft was once a small company really like Bazoocam alternative with girls and boys (I know that is hard to imagine today). You might even have called them a small innovative company back in the ’80s. Through the MS-DOS operating system and the BASIC programming language, Microsoft became the de-facto standard running on most PCs. Through smart marketing and a decent product, they were able to leverage their advantage with other software packages including the much loved and often hated Windows operating system. Over time, they were able to muscle out the most competition and their software has become a standard worldwide. 

      Fast forward to today. I think the best illustration of Microsoft is some terrific Apple commercials that depict Apple vs. Microsoft is personified by two people. You know the ones with the cool Apple guy and the nerdy PC guy. In these commercials, you get the feeling that Apple products are cool without hassle. The PC guy makes you feel like PC products (running Windows) are more complex and difficult to work with. 

      Another example is the new Microsoft Zune MP3 player. While I don’t own one, I have read reviews. All the reviews suggest that it is a decent product. However, it fails to be something truly innovative, instead of copying many of the capabilities of the iPod with some improvements. Hardly as innovative as the first iPod. 

      Microsoft faces the same problem that many once-innovative companies face as they grow larger. As the size and complexity of an organization grow, so too does the number of groups that get involved in any process. Decision-making capability typically becomes distributed across many different departments each of whom wants to have input into the final product. Thus, in many larger organizations, innovative ideas get squashed or have so many hands involved that the original concept gets lost or homogenized in the process. This is especially true in public companies who are under pressure to gain revenue as quickly as possible and cut costs at the same time. 

      I do think Microsoft and other large companies have a potential solution to the innovation problem: Create small companies within the larger company. Allow these teams of people the advantages of the resources of the large organization, but give them the freedom to innovate without the corporate bureaucracy. Apple has been able to avoid having to do this because of the dynamic and visionary nature of their CEO Steve Jobs. While Zune has not been a runaway success, Microsoft is on the right path in having appointed J. Allard to lead the team that developed the Zune. J. Allard is like the cool Apple guy personified. He and his team successfully created the X box 360 and will likely continue to improve the likelihood of success of the Zune over time. 

      This type of strategy is very difficult to institute for a large public company. So much of many larger companies' corporate DNA surrounds hierarchy and control, that it is difficult to delegate decision-making authority to a small group of people. However, companies that do not develop solutions to continue to innovate eventually will wither and disappear. Not only will they struggle in an increasingly competitive marketplace, but they will also seed talent to those companies that continue to provide opportunities to innovate.

      Delete
  2. The web site is lovingly serviced and saved as much as date. So it should be, thanks for sharing this with us
    wuxiaworld

    ReplyDelete
  3. Don't know how to hack Snapchat app? Follow these tips. It's not difficult at all!

    ReplyDelete
  4. Wow you have a great blog here

    21 savage songs
    And I also love this category
    post Malone goodbyes


    Thansk for this information

    ReplyDelete
  5. Wow! This can be one particular of the most useful blogs We’ love ever arrive across on this subject. Actually Excellent. I am also a specialist in this topic, therefore, I can understand your effort. Our number one pick for beginners and hobbyists is the Hantek DSO5102P Digital Storage Oscilloscope. Hantek DSO5102P Digital Storage Oscilloscope - It's one of the best entry-level oscilloscopes when it comes to price/quality ratio.

    mcdonalds survey

    ReplyDelete
  6. Contact an online Custom Paper Writing Services, and they deliver entirely Custom Research Papers upon request. Note that the content of Best Online Essay Writing Services is unique and non-plagiarized.

    ReplyDelete
  7. Bandar Judi Bola Online Terbaik-Permainan bola bermain dengan variasi taruhan. Dalam pertandingan yang dimainkan bola online, Anda pasti harus tahu banyak yang paling berbagai jenis yang tersedia. Karena Anda akan menemukan banyak variasi jenis permainan yang ada di sepak Bandar SBOBET online .

    ReplyDelete
  8. When reading the article, make some notes that will help you write a good outline for your article critique. You should understand that making notes when reading the article, you will make your piece well structured and focused on the relevant details https://manyessays.com/article-critique-writing.

    ReplyDelete
  9. You’ve written nice post, I am gonna bookmark this page, thanks for info. I actually appreciate your own position and I will be sure to come back here.
    http://bit.ly/2AEqTlS

    ReplyDelete
  10. The article you have shared here very awesome. I really like and appreciated your work. I read deeply your article, the points you have mentioned in this article are useful
    sonic games

    ReplyDelete
  11. Excellent blog, it’s really helped me a lot, so keep sharing post like this
    Wireshark Alternatives for Android

    ReplyDelete
  12. This is a very interesting post and all the details are in this post are awesome.
    hotmail login

    ReplyDelete
  13. This comment has been removed by the author.

    ReplyDelete
  14. You can tell me any brand osilloscope good to use ?
    - Lidinco -

    ReplyDelete
  15. Hey there! If you see that writing papers is a big problem then I heard that essay writing service help people to solve this problem. There you can find creative definition essay topics

    ReplyDelete
  16. When choosing a handheld oscilloscope, users should pick one with a bandwidth that is five times more than the highest frequency that has to be captured. Another mistaken assumption is that an oscilloscope with a higher sample rate is better than one with a lower sample rate

    click here to download

    ReplyDelete
  17. When you have a great choice for the modern offers
    www.myinstantoffer.com code

    ReplyDelete
  18. Don't call your name when you're not sure. Will go all together to silver roof. Being with someone who has everything, don't be foolish. Love must put in the right place in the world. 1v1 lol slope unblocked

    ReplyDelete
  19. Save your personal information in Wallets. Editing, shred files and clean your Windows History. Your directories are protected using the 256bit Blowfish Encryption method. Features, and deleting files and directories, hide and PasswordProtect files.
    AVS Video Editor Crack 9.1.2.540 Con Keygen Full Download Torrent
    https://nonsugar.info/idm-crack/46880-the-key-of-folder-lock-7-serial.html

    ReplyDelete
  20. Are you looking for the easiest and simplest way to Install WordPress in cPanel?
    Here are your Steps to Install WordPress in cPanel.
    How to install WordPress in CPanel

    ReplyDelete
  21. This is a very informative blog to select Right Handheld Oscilloscope and Oscilloscope purchaser need to read this blog and purchase Right Handheld Oscilloscope accounting to your need. I am a Website Content Writer and this web content help me to write an article on Oscilloscope

    ReplyDelete
  22. Enjoyed reading the article above , really explains everything in detail, the article is very interesting and effective. Thank you and good luck for the upcoming articles
    CRM Solutions

    ReplyDelete
  23. Best picks for SIX vs STA Big Bash League 2020.
    SIX vs STA Probable Playing XIs
    Sydney Sixers vs Melbourne Stars My Dream11 Playing XI

    ReplyDelete
  24. Subscription management software
    Really very happy to say,your post is very interesting to read.I never stop myself to say something about it.You’re doing a great job.Keep it up

    ReplyDelete
  25. House cleaning Perth offers affordable house cleaning services in Perth. Our professional cleaners are ready to clean your house and make it germs free.

    ReplyDelete
  26. Office cleaning Perth is the most reliable and affordable company in Perth which offers the best office cleaning services in Perth.

    ReplyDelete
  27. Kris Ford is an actor with American citizenship. He is both a businessman and a television figure. He became popular for portraying’ Sons of Arms’ in a reality television show. The series was broadcast from 2011 to 2014. It was shown with his gorgeous wife Stephanie Hayden on Discovery Channel.

    ReplyDelete
  28. My father and me were working as seismologists for a state organization, and we would go to radioactive areas, and check for electromagnetive waves or signals there, which would indicate a phenomenon. These kind of projects were important for me, as I would use the findings to write my assignments, and not having the time to do them because of my time spent on my field, my company would hire affordable assignment help just to ensure that I commit my time on the field

    ReplyDelete
  29. Thanks for your posting. Keep posting like this is very helpful for us have found something new in this Article. Btw also visit my website.
    buy logo online

    ReplyDelete
  30. This gadget is very useful for especially electronic students, and they can improve their knowledge and abilities. Its price is reasonable and many students have bought it. Do you like this one? Cheap dissertation writing service.

    ReplyDelete
  31. Thank you for writing and sharing this useful post. You have several motivating points of view that give me pause to study. Cafe Interior Design

    ReplyDelete
  32. My Assignment Services will help you in making the decisions as per your requirement. They will provide you with many benefits. The essays and assignments will have relevant information. No need to worry anymore. If your workload is piling up and has to submit your assignment in less time, then you can get Homework Help from My Assignment Services. This will help you in setting up your priorities.

    ReplyDelete
  33. i really love your blog, thanks for sharing Sad poetry

    ReplyDelete

  34. Very good write-up. I certainly love this website. Thanks! Walmartmoneycard Register

    ReplyDelete
  35. Thank you so much for sharing all this wonderful information !!!! It is so appreciated!! You have good humor in your blogs. So much helpful and easy to read!
    Java Classes in Bangalore

    ReplyDelete
  36. I'm so glad and enjoyed your BLOG, It is very informative on the subject or topic, and Thanks For Sharing this post. I have something to share here
    buy modalert online
    buy artvigil online
    buy waklert online
    buy modvigil online
    buy vilafinil online
    I'm so glad and enjoyed your BLOG, It is very informative on the subject or topic, and Thanks For Sharing this post. I have something to share here
    buy modalert online
    buy artvigil online
    buy waklert online
    buy modvigil online
    buy vilafinil online

    ReplyDelete
  37. Thanks for sharing. By requesting for our DNP Capstone Editing Help, you can boost your chance of submitting a quality DNP capstone project.

    ReplyDelete
  38. lsm99 เว็บบริการ คาสิโนออนไลน์ เว็บเกมที่จะทำให้ทุกท่านสนุกและเพลิดเพลิน ตื่นเต้น เร้าใจ ลุ้นรางวัลใหญ่อาจจะทำให้ท่านรวยในเวลาอันสั้น

    ReplyDelete
  39. Thanks for sharing such quality blog post, I always appreciate rich information based content. Welcome to the most popular escort agency where we unveil our hot and sexy escorts Manchester.

    ReplyDelete
  40. Thanks for sharing such nice blog post. If you are getting bored and want your lonely night turn into joyful, quickly book Airport Escorts in Manchester & Escorts in Manchester City Centre.

    ReplyDelete
  41. Connect Dubai Fun Club for premium Dubai Escorts and entertainment services. You can easily find the best call girls in Dubai on our website

    ReplyDelete
  42. Wonderful blog! This is very informative site. I am totally pleased by your excellent work. Many thanks for sharing. Choose an oscilloscope with faster rise times, higher waveform update rates, greater acquisition memory depth, sufficient number of channels, multiple probing options, and suitable bandwidths. Also, look for advanced application support for troubleshooting and standards compliance. When choosing a handheld oscilloscope, users should pick one with a bandwidth that is five times more than the highest frequency that has to be captured. check this

    ReplyDelete
  43. Keep it up such an amazing work.
    it is useful for me.

    Mens Aviator Jacket

    ReplyDelete
  44. Very useful and valuable details you shared, thanks for the important blog post. It helped me a lot. nice post very informational. Keep blogging. for More Information Click Here:- HP Scanner Not Working Error

    ReplyDelete
  45. Valuable and also a good post, thanks for the share, if you are looking to law dissertation help Uk then just visit our site and get up to 7O off.

    ReplyDelete
  46. Players can go on a nostalgia trip with Friday Night Funkin’. The gameplay is similar to that of retro rhythm games or puzzle games, making it an incredibly easy-to-play game. However, it is still very challenging to play as the songs can vary in rhythm and speed. Have fun!

    ReplyDelete
  47. Hello, thanks for the wonderful post, I like to write a little comment to support you. Check out the best satta king game and win large amount of money by investing very less at satta king. We provide the best satta king game result and charts online.
    satta king 786
    delhi satta king
    black satta king
    play bazaar

    ReplyDelete
  48. It was so good to see you acknowledging this topic, it really feels great. Thanks for sharing such a valuable information which is very hard to find normally. I have subscribed to your website and will be promoting it to my friends and other people as well.Our new website has been launched and we are offering some exciting prices. Check it out now.
    leather jacket

    ReplyDelete
  49. Thank you for posting such a great article! I found your website perfect for my needs.
    Ted lasso jackets

    ReplyDelete
  50. I found this blog. Much appreciation to you for offering to us, I, everything considered, find some new data from your post. to a cerebrum boggling degree satisfying and I to an amazing degree like your article a commitment of Thankfulness is everything
    Southside Serpents Jacket

    ReplyDelete
  51. I found this blog. Much appreciation to you for offering to us, I, everything considered, find some new data from your post. to a cerebrum boggling degree satisfying and I to an amazing degree like your article a commitment of Thankfulness is everything
    Pelle Pelle Pink jacket

    ReplyDelete
  52. Thank you for posting such a great article! I found your website perfect for my needs.
    GAP pullover hoodie

    ReplyDelete
  53. It's encouraging to see that some individuals are still making an effort to manage their websites. I'll make sure to check back in shortly
    Cafe Racer Brown Leather Jacket

    ReplyDelete
  54. Czech brides have a reasonably adaptable attitude and have no problem comprehending cultures other than their own. When your Czech bride is around, you will always feel welcome as a foreigner. Furthermore, they are fully at ease discussing any subject, including those of a personal character. If you wish to meet such females, you should contact https://toprussianbrides.com/czech-brides/ these guys.

    ReplyDelete
  55. Thank you so much for such a well-written article.
    เกมส์ pg slot

    ReplyDelete
  56. Hello, thank you for sharing your article with us; I value your information, which I greatly value, and I would return to your websitegenuine leather online shop

    ReplyDelete
  57. Thank you for another great article. Where else could anyone get that kind of information in such a perfect way of writing? I have a presentation next week, and I am on the look for such information. Kindly Visit our Website:- Change AT&T Wi-Fi Password

    ReplyDelete
  58. I am glad to discover this page. I have to thank you for the time I spent on this especially great reading !!
    coupon berrylook

    ReplyDelete
  59. Paintless dent removal service in the Bay Area offers consumers all the benefits of a body repair shop but with less hassle, lower costs, and increased quality. Whether your vehicle has a minor dent to the body, scratches due to normal wear and tear, or any other minor ding in need of touch-up paint, you can eliminate some of the biggest burdens of car repair by taking advantage of mobile paintless dent removal services in California. car specs by reg

    ReplyDelete
  60. This is the geat initiative taken as it makes all the researchers explore new ideas and share their prespective along with their collegues Fur Leather Jacket

    ReplyDelete
  61. The content is utmost interesting! I have completely enjoyed reading your points and have come to the conclusion that you are right about many of them. You are great - Crate And Barrel

    ReplyDelete
  62. We know that late assignment submission how can effect on grades. For that reason, assignment help services ensure the timely submission of assignments with authentic and fresh content.

    ReplyDelete
  63. Great goods from you, man. I’ve understand your stuff previous to and you’re just extremely great. I really like what you have acquired here, really like what you’re stating and the way in which you say it. You make it entertaining and you still take care of to keep it sensible. I cant wait to read much more from you. This is really a wonderful website. Best mattress 2022

    ReplyDelete
  64. Appreciative for sharing an especially confounding post. It was really helpful. Keep on sharing more substance
    Red Notice Brownn Jacket

    ReplyDelete
  65. Thank you for sharing informative post with us. You select the best topic for writing. Moreover, The painting contractors Miami are a popular choice because of their high level of work.

    ReplyDelete
  66. Additionally, you can make a booking anytime of the night or day we make it easy to make it easy for you to book the most desirable models for your special occasion in rudrapur. With our 24/7 operating hours, it won't matter when you decide to meet with one of our models. You'll also have an enjoyable and stimulating time thanks to our fantastic models. They won't be missed in a flash.
    what's app rudrapur girls number
    phone call lucknow girls
    hot call Mount Abu girls number.
    call dehradun girls phone number
    call haridwar girls phone number
    what's app beawar girls number

    ReplyDelete
  67. Plumbing Services in California are needed in many cases to keep your home or office functioning at the optimum level. There are many different types of plumbing services that are available to suit your needs if you have a plumbing problem.

    ReplyDelete
  68. Some companies offer professional cleaning services that come to your company and do all of the work while others will require that employees do the work themselves. The Office Cleaning Services in Hialeah FL deliver the best and valuable work in a short time. There are also janitorial services which will provide all of the equipment necessary so that employees can clean their own offices.

    ReplyDelete
  69. Hi there, I check your blog like every week. Your story-telling style is awesome, keep it up!Mens Aviator Jacket

    ReplyDelete
  70. It's encouraging to see that some individuals are still making an effort to manage their websites. I'll make sure to check back in shortly
    Marlboro Leather Jacket

    ReplyDelete
  71. I was the one who read this article! I hope you'll continue to create content like this to share with everyone! Thank you sincerely! atari breakout

    ReplyDelete
  72. Awesome looking custom outfits we've been selling for our valued customers we're back with more awesome pieces
    Red Notice Brown Jacket

    ReplyDelete
  73. I will bookmark your web site and take the feeds additionally…I am satisfied to search out a lot of helpful information right here in the publish, we want work out more techniques on this regard, thanks for sharing. Amazon Product Photographer.

    ReplyDelete
  74. Extremely decent blog and articles. I am really extremely glad to visit your blog. Presently I am discovered what I really need. I check your blog regularly and attempt to take in something from your blog. Much obliged to you and sitting tight for your new post. women clothing brands in pakistan.

    ReplyDelete
  75. Nice information, valuable and excellent design, as share good stuff with good ideas and concepts, lots of great information and inspiration, both of which I need, thanks to offering such a piece of helpful information here. local seo company.

    ReplyDelete
  76. It is a very impressive blog post, I have read it and found very well written. there are some more posts like this as how to buy video editor and I have bookmarked your page.

    ReplyDelete
  77. Hi, I do believe this is a great site. I stumbledupon it 😉 I will revisit
    yet again since I book-marked it. Money and freedom is the greatest way to change, may
    you be rich and continue to help others.Yellowstone Jackets

    ReplyDelete
  78. Ver well. Keep sharing more. Please also read mine blog and let me know where I can improve.
    cupcake boxes wholesale
    Cake Box Wholesale

    ReplyDelete
  79. Before you’re ready to share some bat puns on Halloween, you need to set the stage. For one, your Halloween party won’t be complete without plenty of bat-inspired
    Marlboro Leather Jacket

    ReplyDelete