Thursday, July 24, 2014

Preventive Maintenance test with Insulation Resistance Test, Part 1


Preventive maintenance is a predetermined task performed based on a schedule and its objective is to keep equipment in good condition to avoid breakdowns.
Insulation resistance testing is commonly performed as part of electrical testing in a preventive maintenance program for rotating machines, cables, switches, transformers, and electrical machinery where insulating integrity is needed. Insulation resistance testing in the preventive maintenance program helps identify potential electrical issues to reduce unpredictable, premature equipment repair and replacement cost.


With properly scheduled monitoring and data collection, this testing can be very useful in analyzing and predicting the current and future behavior of equipment. Early problem detection helps avoid major repairs, resulting in cost savings when compared to a run-to-failure maintenance practice. Preventive maintenance has the added benefit of pre-planning for necessary parts and resources.

This first of three articles will describe what is insulation resistance testing, how it plays a part in preventive maintenance and factors that affect insulation resistance. The second article will focus on the methods of insulation resistance testing1  while the last article will detail test voltage selection guidelines and safety considerations.

1 Consulting the original product/equipment manufacturer for more detailed information is recommended.
 

What is Insulation Resistance Testing?
Insulation resistance is used to verify the integrity of the insulation material. It can be the cable insulation or motor/generator winding insulation. Insulation resistance testing is carried out by applying a constant voltage to the equipment under test while measuring the any flowing current. High DC voltages are used causing a small current to flow through the insulator surface. The total current consists of three components: capacitance charging current, absorption current, and leakage current (refer to Figure 1.)


  • Capacitance charging current is relatively high upon start-up and drop exponentially within a few seconds to a few ten seconds. It is normally negligible when the reading is taken.
  • Absorption current decays at a decreasing rate. It may require up to a few minutes to reach zero depending on the insulation materials.
  • Leakage current is constant over time.
Figure 1 Components of test current
How Insulation Resistance Testing Helps in Preventive Maintenance
For an effective test, results should be regularly recorded over a period of time and compared with earlier recorded values taken when the equipment was new and in good condition. The trend of the readings over a period of time will help identify the presence of anomalies. Insulation resistance values that are consistent over time indicate that the equipment’s insulation properties are good. If the resistance values are decreasing, it indicates that potential issues can occur sometime in the future and more thorough preventive maintenance should be scheduled soon.

Factors That Affect the Insulation Resistance
The factors that commonly affect the insulation resistance are:
  • Surface condition. For example oil or carbon dust on the equipment’s surface that can lower the insulation resistance.
  • Moisture. If the equipment’s surface temperature is at, or below, the dew point of the ambient air, a film of moisture forms on its surface would, lowering the equipment’s resistance value.
  • Temperature. The insulation resistance value may vary inversely with the change of the temperature. Its influence on readings can be mitigated by performing preventive maintenance testing at the same temperature each time. If the temperature cannot be controlled, normalizing to a base temperature such as 40 °C is recommended. This is commonly done using the estimation rule, “Every 10 °C increase in temperature halves the insulation resistance, while a 10 °C reduction doubles the resistance”.  As different materials may have different degrees of resistance change due to temperature, for more precise temperature correction, some may adopt a temperature correction factor the measurement reading should be multiplied by multiplying the measurement reading with the temperature correction factor at the corresponding temperature.

In the next article (Part 2), I will cover the insulation resistance test methods.

42 comments:

  1. it can be scary the first time you try this. Just remember, somebody, just like you, insulation blower

    ReplyDelete
  2. With the headway in innovation, programming download sites are likewise on increment and it is hard to find out which ones are veritable and which ones are fake. navigate here

    ReplyDelete
  3. I found that site very usefull and this survey is very cirious, I ' ve never seen a blog that demand a survey for this actions, very curious... attic insulation removal and replacement

    ReplyDelete
  4. thanks for this post.
    Get Online Custom Essay Help at https://assignmentfirm.com/essay-help/online-custom-essay-help.php

    ReplyDelete
  5. Hey,
    I am an academic writer at Online Assignment Expert. I am a regular reader of your blog and article. I really found it quite amazing, informative and interesting as well. I like the way you organise the content and the sources you use to find information and data. Anyhow, I am here to inform the students studying at Australian colleges or universities that we are offering accounting assignment help. Students who encounter problems in doing their assignment or need any type of other assistance can contact us. You will find a team of academic writers who have completed their studies from the most reputed college and university. They are here to deliver an errorless and genuine accounting assignment help service.
    Our assignment expert holds a PhD degree in the field of accounting and finance. They have years of experience in producing assignments for accounting.
    Therefore, in case you need assistance from the services like assignment help Australia visit our official website.

    ReplyDelete
  6. Highly recommend to see the collection of the best cell phone tracking applications. They are reliable and effective.

    ReplyDelete
  7. Hey! Thank you for providing us with such an informational blog. This is indeed helpful. My Assignment Services also assists students who struggle to complete their assessments on time. Our Catia assignment help is a unique academic service designed specially for those who are studying this unit. We have a whole team of certified Catia assignment writers who have been using the CATIA CAD software since it was first launched. These experts are also well-versed with other CAD software such as STATA, AutoCAD, and many more. With their high-level of knowledge and years of expertise, students often consider them as the best STATA assignment help providers in Australia. Thus, we’re always there whenever students find challenges in writing their STATA and CATIA assignments. They can also avail of full-solved assignment samples from us and use them to prepare their own assessment tasks easily. With our STATA assignment help, scoring the top grades is more achievable than ever!

    ReplyDelete
  8. QuickBooks is a widely used Accounting Software. It solves all the accounting solution of your business. If you are using QuikBooks Software and need any kind of assistance related to the software then you can contact to QuickBooks Support for help.

    ReplyDelete
  9. As much as a Research Papers for Saleis a summary of other works that should not be an excuse to make papers with College Research Papers for Sale.

    ReplyDelete
  10. It is understandable that one is more confident when their task is in the hands of the Order College Research Papers than a novice; thus, one hires Custom College Research Papers Writer who delivers the ideal Legitimate College Research Paper.

    ReplyDelete
  11. Do you require Top Homework Writing Services for your assignments’ needs, but you are unsure of the Best Homework Writing firm to contract? Our Custom Essay Writing Company has credibility and has been providing homework solutions.

    ReplyDelete
  12. You’ve written nice post, I am gonna bookmark this page, thanks for info. I actually appreciate your own position and I will be sure to come back here.
    red ball

    ReplyDelete
  13. The article you have shared here very awesome. I really like and appreciated your work. I read deeply your article, the points you have mentioned in this article are useful
    red ball

    ReplyDelete
  14. Awesome! I love this fruitful content. Thanks for your time
    9CHAT For PC

    ReplyDelete
  15. This game is currently being released, but it became more popular in less time, this will be the most effective game for those who have more ideas when you start playing this game. Play download tweakbox y8 game

    ReplyDelete
  16. Preventive maintenance Plan is scheduled, routine maintenance to keep equipment ... It can also save on maintenance costs because the system can plan.


    Preventive maintanance plan
    Agaram infotech

    ReplyDelete
  17. A preventive maintenance plan (sometimes called 'preventative maintenance programs') attempts to help you proactively perform maintenance, repairs, and replacements so that you can prevent failures before they ever have the chance to occur.


    Preventive maintanance plan
    Agaram infotech

    ReplyDelete
  18. Looking for Local Plumber Near Me services on web Local Plumber Near Me, Our professional plumbers are there to assist the commercial caretakers and residents.

    ReplyDelete
  19. With properly scheduled monitoring and data collection, this testing can be very useful in analysing and predicting the current and future behaviour of equipment. Early problem detection helps avoid major repairs, resulting in cost savings when compared to a run-to-failure maintenance practice.

    John,
    @ Write My Essay

    ReplyDelete
  20. Preventive maintenance that includes insulation resistance testing gives maintenance managers more control over electric motor systems.

    kahootsmasher apkxyz

    ReplyDelete
  21. Of course, there should be more attention paid to the issue of cyberbullying and the overall safety of our children. Recently, I started using mspy phone tracking app, and now, I can see where my child is and even monitor his calls and messages. I can block an suspicious caller anytime, and that's a huge relief.

    ReplyDelete
  22. I read this article! I hope you will continue to have such articles to share with everyone! thank you!
    Screencastify

    ReplyDelete
  23. To be honest I found very helpful information your blog thanks for providing us such blog

    Url Video Player For PC

    ReplyDelete
  24. This is extremely helpful info!! Very good work. Everything is very interesting to learn and easy to understood. Thank you for giving information.
    url

    ReplyDelete
  25. It is important to seek english language essay writing services and english language coursework writing services since students find help when they visit English Language Writing Services.

    ReplyDelete
  26. This will be all you want visit here it is very interesting and fascinating.

    ReplyDelete
  27. du hoc canada vnsava
    Chuyên du học Canada Công ty tư vấn du học Canada nào tốt
    Điều kiện du học Canada 2021
    Học bổng du học Canada vnsava

    vnsava
    Thông tin du học Canada mới nhất

    vnsava
    Chính sách du học Canada 2020
    vnsava
    Du học Canada bao nhiêu tiền Việt
    Học bổng du học Canada 2020
    vnsava
    Du học Canada 2020
    Nhất ký du học Canada
    vnsava
    Du học Canada nên học ngành gì
    công ty tư vấn du học Canada vnsava, chính sách điều kiện định cư Canada, học bổng, chi phí, điều kiện xin visa canada
    #vnsava
    @vnsava
    vnsava
    vnsava
    vnsava

    ReplyDelete
  28. We are one among the web design and development company. Our objective is to deliver clients with trending solutions that add values to their webpages and applications. We are Professional Website Design Services and we have efficient team of experts who are keen to complete the project within specified period. Our HTML5 developers are up to date in latest designing tools and technologies to build interactive websites. If you are looking for professional web design company also you can hire web designer we are here to help you.

    ReplyDelete
  29. It is important to seek statistics coursework writing services and statistics essay writing services since students find help when they visit Business Statistics Writing Services.

    ReplyDelete
  30. Thanks for sharing this phenomenal post. I must say i enjoyed scanning this wonderful post. It had been very informative and helpful post you tell us, continue to good work. Please visit Call Girls in Kolkata to know why The Call girls in Kolkata are known for their dusky and fair skin tone and you can take the service from any of them according to your wish.

    call girls in Kolkata
    Kolkata call girls
    call girl services in Kolkata
    Kolkata call girl services
    call girl agency in Kolkata
    Kolkata call girls agency
    call girl agencies in Kolkata
    Kolkata call girl agencies
    independent call girls in Kolkata
    independent Kolkata call girls
    escorts in Kolkata
    Kolkata escorts
    independent escorts in Kolkata
    independent Kolkata escorts


    ReplyDelete
  31. It is important to seek sociology paper writing services and sociology assignment writing services since students find help when they visit Sociology Essay Writing Services.

    ReplyDelete