Thursday, January 1, 2015

Tips: Capturing crisp and clear infrared thermal image

Happy New Year, readers! I wanted to start the year by sharing some useful tips on how you can capture crisp and clear infrared thermal image. Thermal imagers or thermal cameras available on the shelf today are quite intuitive and easy to use. However, getting the best thermal image and then interpreting it later requires knowledge and experience. Here are some tips that can help you be better prepared when you are out in the field.
  1. Get the right focus on the target area for more accurate temperature readings. There are several types of focusing mechanism available – fixed-focus, manual focus or auto focus, with the latter being the most advanced. Take your time to get it right at this stage because this cannot be edited later!
  2. Perform a quick scan on the targeted area that you are inspecting. Set both the temperature range and scale to auto mode, to quickly get the temperature range of the area. Once done, you can fix the temperature scale by enabling the manual mode, to capture a more stable image. Change the mode quickly with the Auto/Man quick access- button (press-and-hold) on the U5855A TrueIR thermal imager.
  3. Once a suspected hotspot is found, manually refocus on the hot spot area. Always validate if it is a real hotspot by checking for any possible reflective heat sources or solar loading effect, if the inspection is done in an open area or under the sunlight. Move from side to side to eliminate possible external or reflective heat sources.
  4. Check the surface condition and material of the hotspot area and apply a suitable emissivity coefficient factor, Ɛ. Note: If the object’s surface is polished or shiny in nature, both the Ɛ and emitted IR energy will be low. These surfaces can also reflect IR energy from other sources. In such cases, the low Ɛ and external reflected IR energy typically produces an inaccurate temperature measurement. Ensure these values are compensated by setting the right reflected temperature, ambient temperature and humidity of the area of inspection.
  5. Capture and save the IR image for reporting purposes. Extra identification and information on the hotspot area can be done by note/photo tagging (with TrueIR thermal imager, user can capture and tag up to 3 visible photos to each of the infrared images captured) or with simply writing it down in notebook.
Sample infrared thermal image of electronics PCB board
taken with U5855A TrueIR thermal imager








Sample infrared thermal image of solar panels
taken with U5855A TrueIR thermal imager



Perform post-IR thermography analysis, such as adding additional temperature spot measurements, box measurements,line or histogram analysis to further support the findings. Correction parameters, such as emissivity, reflected & ambient temperatures as well as color alarm setting can also be done during post-analysis. TrueIR thermal imager comes with free downloadble software  (www.keysight.com/find/TrueIR_ART) that can be used for analysis and reporting purposes.  





39 comments:

  1. Replies
    1. Technology is good and I think it will get famous soon because it is something very unique and every unique idea get famous in quick time and those who wants to get immigration service they must need to know first Quebec immigration requirements before avail this service by any other service providers

      Delete
    2. I really liked your blog amazing ideas I am inspired in many ways. I am searching for the water tank cleaning services sites to get such services for making my problem solved. I am read your site in my free time to get more informative ideas.

      Delete
  2. Replies
    1. As we see many new students getting enrolment in universities and institutes. it helps to online test takers on the websites. Many students are giving test online for checking how much they studied by doing they can easily know the result.

      Delete
  3. Thanks for your sharing about capturing crisp and clear infrared thermal image.
    madalin stunt cars 2 unblocked

    ReplyDelete
  4. Jobs divine is one of the top job consultancy in thrissur. We provide all types of jobs in thrissur. We do have many job vacancies in thrissur. Sign up now for a free account and get thrissur jobs instantly. The candidates who in search of good career in Thrissur can apply and get easily their dream job through jobs divine

    ReplyDelete
  5. Thank you so much for posting this. If you are a university students in need dissertation help, then you can surely visit Assignment Help UK to take further guidance about your dissertation writing work.

    ReplyDelete
    Replies
    1. This blog page contains a lot of information. Personally I really need to know about infrared thermal image because I have an assignment want to take some online help by uk dissertation help - AceMyAssignment professionals. Infrared is a kind of rays that are invisible to us but we can feel these rays as heat.

      Delete
  6. That is one important information for me.
    super smash flash 2

    ReplyDelete

  7. I love what you guys tend to be up too. This type of clever work and reporting!
    Keep up the amazing works guys I’ve included you guys to our blogroll.

    gmail login

    ReplyDelete
  8. Wow, nice blog , I love this blog seriously, and you can follow us @ Fulloaded


    And also Download Latest Naija Music

    Even you can visit our Naija Freebeat

    ReplyDelete
  9. Contact us for best price and deals ever

    Weblink:https://www.elightdocumentation.com
    Email: elightdocumentation@gmail.com
    Whatsapp No: +1 (318) 500-3487
    product link:https://www.elightdocumentation.com/grade-aa-fake-euro-for-sale/
    https://www.supercounterfeitbills.com
    https://www.bestqualitynotes.com
    https://www.flymedishop.com
    https://www.buymoneybills.com
    productlink.. https://www.elightdocumentation.com/where-to-buy-the-best-counterfeit-money/
    productlink.. https://www.elightdocumentation.com/grade-aa-fake-euro-for-sale/
    productlink.. https://www.elightdocumentation.com/buy-counterfeit-mexican-peso-online/
    productlink.. https://www.elightdocumentation.com/the-best-counterfeit-money-sale/

    Buy Counterfeit Mexican Peso Online

    Buy Counterfeit Mexican Peso Online. While our counterfeit currency is
    top-notch,
    you shouldn’t risk more than you need to. Don’t use fake money at any place that
    has professionals who can determine whether a banknote is fake or not.
    If you try to pay a fine with counterfeits, there is a high chance you will
    be caught pretty soon.

    What you should do instead is to pay for regular purchases in places
    where no one
    cares enough to check the money. Mix the real and the fake banknotes to lessen
    the chances of being caught even further. The two will look alike, however.
    Place an order now, and you can see it for yourself. Buy Counterfeit Mexican
    Peso Online
    Buy Counterfeit Mexican Peso Online

    Contact us for best price and deals ever

    Weblink:https://www.elightdocumentation.com
    Email: elightdocumentation@gmail.com
    Whatsapp No: +1 (318) 500-3487
    product link:https://www.elightdocumentation.com/buy-counterfeit-mexican-peso-online/
    https://www.supercounterfeitbills.com
    https://www.bestqualitynotes.com
    https://www.flymedishop.com
    https://www.buymoneybills.com
    productlink.. https://www.elightdocumentation.com/where-to-buy-the-best-counterfeit-money/
    productlink.. https://www.elightdocumentation.com/grade-aa-fake-euro-for-sale/
    productlink.. https://www.elightdocumentation.com/buy-counterfeit-mexican-peso-online/
    productlink.. https://www.elightdocumentation.com/the-best-counterfeit-money-sale/

    ReplyDelete
  10. Click download snaptubbe to play an interesting and exciting game that we bring to you.

    ReplyDelete
  11. I think it is a good idea, I have thought of it but not as detailed as you. Election Fighting

    ReplyDelete
  12. It's very good post which I really enjoyed reading. It is not everyday that I have the possibility to see something like this.
    gem swap 2

    ReplyDelete
  13. Things are very open and intensely clear explanation of issues. was truly information. Your website is very beneficial.

    Disney Magic Kingdoms

    ReplyDelete
  14. Essay on health & nutrition writing services are essential for college nutrition coursework writing services seekers and Nutrition Research Paper Services.

    ReplyDelete
  15. If I had read your article earlier, it would have been different. My ideas will definitely become more complete if you add your comments. It's so wonderful download android apk

    ReplyDelete
  16. Much thanks to you such a great amount for posting this. On the off chance that you are a college understudies in need exposition help, premiumdissertation.co.uk at that point you can without a doubt visit Assignment Help UK to take further direction about your paper composing work.

    ReplyDelete
  17. Auto center can accelerate the centering procedure, while as yet getting exact core interest. Be that as it may, there are constraints. Self-adjust doesn't permit the thermographer to pick which focus on the camera Online Dissertation Help should concentrate on. As there are regularly numerous expected focuses in a field of view, the camera may concentrate on some different option from the proposed target, so manual change is frequently still important.

    ReplyDelete
  18. I really like reading through a post that can make people think
    play vex 3

    ReplyDelete
  19. Write for us Digital Marketing for SEM Updates - advanced advertising blog? We acknowledge visitor posts for sem, ppc, advanced advertising, marking, online life and more.

    ReplyDelete
  20. The Article is wrapped very nicely, thanks for sharing it. Do you know about Sapiyo.com from where you can buy Instagram followers to increase the number of audience approaching your profile day by day.

    ReplyDelete
  21. I appreciate your hard work. Keep posting new updates with us. This is really a wonderful post. Nice Blog Very interesting and useful information on your website. Thanks for sharing the blog and this great information which is definitely going to help us.
    office.com/setup
    office.com/setup

    ReplyDelete
  22. Faded letters Love story do not know where Nobody wants to forget quickly Can't see each other. geometry dash

    ReplyDelete
  23. Students often have to deal with tough schedules and never-ending deadlines. The best Dissertation Help Online is the brand that is dedicated towards earning the satisfaction of its thousands of student customers worldwide with each order being delivered. Our services are available at affordable rates and they delivered unmatched work quality.

    ReplyDelete
  24. Thanks for sharing this phenomenal post. I must say i enjoyed scanning this wonderful post. It had been very informative and helpful post you tell us, continue to good work. Please visit Call Girls in Kolkata to know why The Call girls in Kolkata are known for their dusky and fair skin tone and you can take the service from any of them according to your wish.

    call girls in Kolkata
    Kolkata call girls
    call girl services in Kolkata
    Kolkata call girl services
    call girl agency in Kolkata
    Kolkata call girls agency
    call girl agencies in Kolkata
    Kolkata call girl agencies
    independent call girls in Kolkata
    independent Kolkata call girls
    escorts in Kolkata
    Kolkata escorts
    independent escorts in Kolkata
    independent Kolkata escorts


    ReplyDelete
  25. Hi, keep up the good work. I prefer the seek thermal camera, higher resolution sensor then the FLIR and doesn't need charging. write my assignment cheap

    ReplyDelete