Previous part
covers the introduction of the printed circuit board assembly troubleshooting
can be found here.
Circuit
board failures may be caused by overheated components such as power transistors
and ICs. Traditionally, overheated components are detected by simply touching
the surface component. This can be dangerous and has to be done with extreme
caution to avoid getting burnt fingers and electrocuted. For circuit boards
suspected of thermal failures, they can be detected for hotspots using an IR
thermal imager without physically touching the components. Infrared thermal
imaging is able to capture the temperature distribution of the whole circuit which
makes it easy to see the hotspot at a glance.
![]() |
Figure 2 Detecting
hotspot on a circuit board using Keysight U5850 series TrueIR Thermal Imagers with image logging capability
|
Typically,
320 x 240 pixels of in-camera fine resolution such as Keysight U5850 series
TrueIR Thermal Imagers with the
ability to focus on objects as close as 10 cm, are idea for measuring temperature
of small components that are close to each other. Additionally, the thermal
imager monitors temperature changes through image logging and temperature
trending capabilities using the TrueIR
Analysis and Reporting Tool software.
For
more accurate temperature monitoring, the component temperature can be measured
using a Keysight digital multimeter with a thermocouple probe attached to the
surface of the component while the circuit board is powered on.
![]() |
Figure 3 Monitoring
the temperature of a circuit board with the U1282A handheld digital multimeter
|
Next, we will talk
about how to detect faulty components during PCBA troubleshooting using a handheld
digital multimeter.
Excellent information on your blog, thank you for taking the time to share with us. Amazing insight you have on this, it's nice to find a website that details so much information about different artists. Digital Marketing KC
ReplyDeleteI think this is an informative post and it is very useful and knowledgeable. therefore, I would like to thank you for the efforts you have made in writing this article. Vegas SEO Company
ReplyDeleteGreat Post!Very Informative Post
ReplyDeleteMake My Assignment
Nice post.
ReplyDeleteBiology Assignment Help
Nice Blog!Keep Sharing With Us
ReplyDeleteRisk Management Assignment Help